ACTION#.CONDITIONVALUE

Description

ACTION#.CONDITIONVALUE defines the value used by ACTION#.CONDITION to test against the source. The range of this keyword depends on the value of ACTION#.SOURCE and ACTION#.CONDITION. Both must be set before setting the condition value. If ACTION#.CONDITION is modified, the range of the ACTION#.CONDITIONVALUE may change, and the value will return to default.

Some conditions do not require a condition value.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

N/A

Range

Depends on ACTION#.SOURCE and ACTION#.CONDITION

Default Value

Depends on ACTION#.SOURCE and ACTION#.CONDITION

Data Type

Float

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

ACTION1.CONDITIONVALUE

3902h

01h

Signed32

-

1000:1

Read/Write

No

ACTION2.CONDITIONVALUE

3902h

02h

Signed32

-

1000:1

Read/Write

No

ACTION3.CONDITIONVALUE

3902h

03h

Signed32

-

1000:1

Read/Write

No

ACTION4.CONDITIONVALUE

3902h

04h

Signed32

-

1000:1

Read/Write

No

ACTION5.CONDITIONVALUE

3902h

05h

Signed32

-

1000:1

Read/Write

No

ACTION6.CONDITIONVALUE

3902h

06h

Signed32

-

1000:1

Read/Write

No

ACTION7.CONDITIONVALUE

3902h

07h

Signed32

-

1000:1

Read/Write

No

ACTION8.CONDITIONVALUE

3902h

08h

Signed32

-

1000:1

Read/Write

No

ACTION9.CONDITIONVALUE

3902h

09h

Signed32

-

1000:1

Read/Write

No

ACTION10.CONDITIONVALUE

3902h

0ah

Signed32

-

1000:1

Read/Write

No

ACTION11.CONDITIONVALUE

3902h

0bh

Signed32

-

1000:1

Read/Write

No

ACTION12.CONDITIONVALUE

3902h

0ch

Signed32

-

1000:1

Read/Write

No

ACTION13.CONDITIONVALUE

3902h

0dh

Signed32

-

1000:1

Read/Write

No

ACTION14.CONDITIONVALUE

3902h

0eh

Signed32

-

1000:1

Read/Write

No

ACTION15.CONDITIONVALUE

3902h

0fh

Signed32

-

1000:1

Read/Write

No

ACTION16.CONDITIONVALUE

3902h

10h

Signed32

-

1000:1

Read/Write

No

ACTION17.CONDITIONVALUE

3902h

11h

Signed32

-

1000:1

Read/Write

No

ACTION18.CONDITIONVALUE

3902h

12h

Signed32

-

1000:1

Read/Write

No

ACTION19.CONDITIONVALUE

3902h

13h

Signed32

-

1000:1

Read/Write

No

ACTION20.CONDITIONVALUE

3902h

14h

Signed32

-

1000:1

Read/Write

No

ACTION21.CONDITIONVALUE

3902h

15h

Signed32

-

1000:1

Read/Write

No

ACTION22.CONDITIONVALUE

3902h

16h

Signed32

-

1000:1

Read/Write

No

ACTION23.CONDITIONVALUE

3902h

17h

Signed32

-

1000:1

Read/Write

No

ACTION24.CONDITIONVALUE

3902h

18h

Signed32

-

1000:1

Read/Write

No

ACTION25.CONDITIONVALUE

3902h

19h

Signed32

-

1000:1

Read/Write

No

ACTION26.CONDITIONVALUE

3902h

1ah

Signed32

-

1000:1

Read/Write

No

ACTION27.CONDITIONVALUE

3902h

1bh

Signed32

-

1000:1

Read/Write

No

ACTION28.CONDITIONVALUE

3902h

1ch

Signed32

-

1000:1

Read/Write

No

ACTION29.CONDITIONVALUE

3902h

1dh

Signed32

-

1000:1

Read/Write

No

ACTION30.CONDITIONVALUE

3902h

1eh

Signed32

-

1000:1

Read/Write

No

ACTION31.CONDITIONVALUE

3902h

1fh

Signed32

-

1000:1

Read/Write

No

ACTION32.CONDITIONVALUE

3902h

20h

Signed32

-

1000:1

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

40300

1

40300 (0x9d6c)

ACTION1.CONDITIONVALUE

Signed32

Read/Write

Yes

40301

1

40301 (0x9d6d)

ACTION2.CONDITIONVALUE

Signed32

Read/Write

Yes

40302

1

40302 (0x9d6e)

ACTION3.CONDITIONVALUE

Signed32

Read/Write

Yes

40303

1

40303 (0x9d6f)

ACTION4.CONDITIONVALUE

Signed32

Read/Write

Yes

40304

1

40304 (0x9d70)

ACTION5.CONDITIONVALUE

Signed32

Read/Write

Yes

40305

1

40305 (0x9d71)

ACTION6.CONDITIONVALUE

Signed32

Read/Write

Yes

40306

1

40306 (0x9d72)

ACTION7.CONDITIONVALUE

Signed32

Read/Write

Yes

40307

1

40307 (0x9d73)

ACTION8.CONDITIONVALUE

Signed32

Read/Write

Yes

40308

1

40308 (0x9d74)

ACTION9.CONDITIONVALUE

Signed32

Read/Write

Yes

40309

1

40309 (0x9d75)

ACTION10.CONDITIONVALUE

Signed32

Read/Write

Yes

40310

1

40310 (0x9d76)

ACTION11.CONDITIONVALUE

Signed32

Read/Write

Yes

40311

1

40311 (0x9d77)

ACTION12.CONDITIONVALUE

Signed32

Read/Write

Yes

40312

1

40312 (0x9d78)

ACTION13.CONDITIONVALUE

Signed32

Read/Write

Yes

40313

1

40313 (0x9d79)

ACTION14.CONDITIONVALUE

Signed32

Read/Write

Yes

40314

1

40314 (0x9d7a)

ACTION15.CONDITIONVALUE

Signed32

Read/Write

Yes

40315

1

40315 (0x9d7b)

ACTION16.CONDITIONVALUE

Signed32

Read/Write

Yes

40316

1

40316 (0x9d7c)

ACTION17.CONDITIONVALUE

Signed32

Read/Write

Yes

40317

1

40317 (0x9d7d)

ACTION18.CONDITIONVALUE

Signed32

Read/Write

Yes

40318

1

40318 (0x9d7e)

ACTION19.CONDITIONVALUE

Signed32

Read/Write

Yes

40319

1

40319 (0x9d7f)

ACTION20.CONDITIONVALUE

Signed32

Read/Write

Yes

40320

1

40320 (0x9d80)

ACTION21.CONDITIONVALUE

Signed32

Read/Write

Yes

40321

1

40321 (0x9d81)

ACTION22.CONDITIONVALUE

Signed32

Read/Write

Yes

40322

1

40322 (0x9d82)

ACTION23.CONDITIONVALUE

Signed32

Read/Write

Yes

40323

1

40323 (0x9d83)

ACTION24.CONDITIONVALUE

Signed32

Read/Write

Yes

40324

1

40324 (0x9d84)

ACTION25.CONDITIONVALUE

Signed32

Read/Write

Yes

40325

1

40325 (0x9d85)

ACTION26.CONDITIONVALUE

Signed32

Read/Write

Yes

40326

1

40326 (0x9d86)

ACTION27.CONDITIONVALUE

Signed32

Read/Write

Yes

40327

1

40327 (0x9d87)

ACTION28.CONDITIONVALUE

Signed32

Read/Write

Yes

40328

1

40328 (0x9d88)

ACTION29.CONDITIONVALUE

Signed32

Read/Write

Yes

40329

1

40329 (0x9d89)

ACTION30.CONDITIONVALUE

Signed32

Read/Write

Yes

40330

1

40330 (0x9d8a)

ACTION31.CONDITIONVALUE

Signed32

Read/Write

Yes

40331

1

40331 (0x9d8b)

ACTION32.CONDITIONVALUE

Signed32

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

ACTION1.CONDITIONVALUE

40300

Float

Read/Write

-

ACTION2.CONDITIONVALUE

40301

Float

Read/Write

-

ACTION3.CONDITIONVALUE

40302

Float

Read/Write

-

ACTION4.CONDITIONVALUE

40303

Float

Read/Write

-

ACTION5.CONDITIONVALUE

40304

Float

Read/Write

-

ACTION6.CONDITIONVALUE

40305

Float

Read/Write

-

ACTION7.CONDITIONVALUE

40306

Float

Read/Write

-

ACTION8.CONDITIONVALUE

40307

Float

Read/Write

-

ACTION9.CONDITIONVALUE

40308

Float

Read/Write

-

ACTION10.CONDITIONVALUE

40309

Float

Read/Write

-

ACTION11.CONDITIONVALUE

40310

Float

Read/Write

-

ACTION12.CONDITIONVALUE

40311

Float

Read/Write

-

ACTION13.CONDITIONVALUE

40312

Float

Read/Write

-

ACTION14.CONDITIONVALUE

40313

Float

Read/Write

-

ACTION15.CONDITIONVALUE

40314

Float

Read/Write

-

ACTION16.CONDITIONVALUE

40315

Float

Read/Write

-

ACTION17.CONDITIONVALUE

40316

Float

Read/Write

-

ACTION18.CONDITIONVALUE

40317

Float

Read/Write

-

ACTION19.CONDITIONVALUE

40318

Float

Read/Write

-

ACTION20.CONDITIONVALUE

40319

Float

Read/Write

-

ACTION21.CONDITIONVALUE

40320

Float

Read/Write

-

ACTION22.CONDITIONVALUE

40321

Float

Read/Write

-

ACTION23.CONDITIONVALUE

40322

Float

Read/Write

-

ACTION24.CONDITIONVALUE

40323

Float

Read/Write

-

ACTION25.CONDITIONVALUE

40324

Float

Read/Write

-

ACTION26.CONDITIONVALUE

40325

Float

Read/Write

-

ACTION27.CONDITIONVALUE

40326

Float

Read/Write

-

ACTION28.CONDITIONVALUE

40327

Float

Read/Write

-

ACTION29.CONDITIONVALUE

40328

Float

Read/Write

-

ACTION30.CONDITIONVALUE

40329

Float

Read/Write

-

ACTION31.CONDITIONVALUE

40330

Float

Read/Write

-

ACTION32.CONDITIONVALUE

40331

Float

Read/Write

-